API Plan 23
Kit components shown solid and include some optional components.
API Plan 23
API Plan 23 utilizes a circulation device, typically a pumping ring, to route the fluid from the seal chamber through a cooler before returning the cooled fluid to the seal chamber. A throat bushing isolates the cooled seal chamber flush fluid from the hotter pumped liquid.
This plan:
- Provides an isolated cooled flush fluid in the seal chamber
- Reduces cooler duty due to isolated flush fluid, extending the life of the close-clearance throat bushing
Plan 23 is available as a kit of components ready for field assembly. Kit contents may include:
- Swagelok tube fittings
- Pipe fittings
- V series 2-valve manifold
- 63 series ball valves
- Bimetal thermometer
- TTW series thermowell tee
- PGI series gauges
- Tubing Pressure transmitter
- Heat exchanger
- Heat exchanger stand
- Pipe nipple
See page 23 of the Mechanical Seal Support Systems Application Guide for additional details and ordering information. Contact Swagelok Allentown for information on optional components.